Solid Edge FrameworkSupport Type Library
IsMember Property
Description
This read-only Boolean property returns True if the object specified is a member of the referenced BoltHoleCircle object.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsMember( _
   ByVal Object As Object, _
   Optional ByVal Object_Keypoint_Index As Variant _
) As Boolean
Parameters
Object
Object_Keypoint_Index
See Also

BoltHoleCircle Collection  | BoltHoleCircle Members

Send comments on this topic.