Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objBounds As SolidEdgeFrameworkSupport.Boundaries2d
    Dim dblPoint(1 To 8) As Double
    Dim lngCount As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'getting the Boundaries2d object on the active sheet
    Set objBounds = objSheet.Boundaries2d
    ' Create a Points array
    dblPoint(1) = 0.1
    dblPoint(2) = 0.2
    dblPoint(3) = 0.3
    dblPoint(4) = 0.35
    dblPoint(5) = 0.4
    dblPoint(6) = 0.1
    dblPoint(7) = 0.25
    dblPoint(8) = 0.1
    ' Create a Boundary2d object
    Call objBounds.AddByPoints(PointCount:=4, Points:=dblPoint)
    ' getting the number of Boundary2d objects in the collection object
    lngCount = objBounds.Count
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objBounds = Nothing
End Sub