Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objBounds As SolidEdgeFrameworkSupport.Boundaries2d
Dim objBound As SolidEdgeFrameworkSupport.Boundary2d
Dim dblPoint(1 To 8) As Double
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Get the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'Get the Boundaries2d object on the active sheet
Set objBounds = objSheet.Boundaries2d
' Create a Points array
dblPoint(1) = 0.1
dblPoint(2) = 0.1
dblPoint(3) = 0.1
dblPoint(4) = 0.2
dblPoint(5) = 0.2
dblPoint(6) = 0.2
dblPoint(7) = 0.2
dblPoint(8) = 0.1
' Create a Boundary2d object
Set objBound = objBounds.AddByPoints(PointCount:=4, Points:=dblPoint)
'Create a Duplicate of the existing boundary
Call objBound.Duplicate(XDistance:=0.1, YDistance:=0.1)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objBounds = Nothing
Set objBound = Nothing
End Sub