Solid Edge FrameworkSupport Type Library
Move Method
Specifies the x coordinate of the origin.
Specifies the y coordinate of the origin.
Specifies the x coordinate of the destination.
Specifies the y coordinate of the destination.
Description
Moves the referenced object.
Syntax
Visual Basic
Public Sub Move( _
   ByVal XFrom As Double, _
   ByVal YFrom As Double, _
   ByVal XTo As Double, _
   ByVal YTo As Double _
) 
Parameters
XFrom
Specifies the x coordinate of the origin.
YFrom
Specifies the y coordinate of the origin.
XTo
Specifies the x coordinate of the destination.
YTo
Specifies the y coordinate of the destination.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objBounds As SolidEdgeFrameworkSupport.Boundaries2d
    Dim objBound As SolidEdgeFrameworkSupport.Boundary2d
    Dim dblPoint(1 To 8) As Double

    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'getting the Boundaries2d object on the active sheet
    Set objBounds = objSheet.Boundaries2d
    ' Create a Points array
    dblPoint(1) = 0.1
    dblPoint(2) = 0.1
    dblPoint(3) = 0.1
    dblPoint(4) = 0.2
    dblPoint(5) = 0.2
    dblPoint(6) = 0.2
    dblPoint(7) = 0.2
    dblPoint(8) = 0.1
    ' Create a Boundary2d object
    Set objBound = objBounds.AddByPoints(PointCount:=4, Points:=dblPoint)

    ' Move the boundry to a new location
    Call objBound.Move(XFrom:=0#, YFrom:=0#, XTo:=0.05, YTo:=0.05)

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objBounds = Nothing
    Set objBound = Nothing
End Sub
See Also

Boundary2d Object  | Boundary2d Members

Send comments on this topic.