| Solid Edge FrameworkSupport Type Library > Boundary2d Object : Style Property |
| Visual Basic |
|---|
Public Property Style As BoundaryStyle2d |
Private Sub Form_Load() Dim objApp As SolidEdgeFramework.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objBounds As SolidEdgeFrameworkSupport.Boundaries2d Dim objBound As SolidEdgeFrameworkSupport.Boundary2d Dim objStyle As SolidEdgeFrameworkSupport.BoundaryStyle2d Dim dblPoint(1 To 8) As Double ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If 'Get the Active Sheet object Set objSheet = objDoc.ActiveSheet 'Get the Boundaries2d object on the active sheet Set objBounds = objSheet.Boundaries2d ' Create a Points array dblPoint(1) = 0.1 dblPoint(2) = 0.1 dblPoint(3) = 0.1 dblPoint(4) = 0.2 dblPoint(5) = 0.2 dblPoint(6) = 0.2 dblPoint(7) = 0.2 dblPoint(8) = 0.1 ' Create a Boundary2d object Set objBound = objBounds.AddByPoints(PointCount:=4, Points:=dblPoint) 'Get Type Set objStyle = objBound.Style ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objBounds = Nothing Set objBound = Nothing Set objStyle = Nothing End Sub