DashName | Sets and returns the named dash style for the referenced object. |
FillColor | Sets and returns the color with which to fill the background of an object. |
FillName | Sets and returns the name of the Fill Style that is associated with the referenced Boundary2d object. |
FillType | Sets and returns the type of the fill style that is associated with the referenced Boundary2d object. |
LinearColor | Sets and returns the group edge color for the referenced style object. |
Rotation | For OLE objects, specifies the angle at which the object is rotated along its major axis. For hatch lines, sets and returns the rotation angle used to display hatch lines. |
Scale | Sets or returns the scale for the referenced object. |
spacing | Sets and returns the distance between the primary hatch lines in a hatch pattern. |
Units | Sets and returns the units in which the line width is defined. |
Width | Returns the width of the referenced object. |