| Solid Edge FrameworkSupport Type Library > CenterMarks Collection : Style Property |
| Visual Basic |
|---|
Public Property Style As DimensionStyle |
Private Sub Form_Load() Dim objApp As SolidEdgeFramework.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objCenterMarks As SolidEdgeFrameworkSupport.CenterMarks Dim objCMStyle As SolidEdgeFrameworkSupport.DimensionStyle ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If ' getting the active sheet Set objSheet = objDoc.ActiveSheet ' getting the CenterMarks collection object on the active sheet Set objCenterMarks = objSheet.CenterMarks ' setting the Style of the CenterMarks collection object objCenterMarks.Style = objDoc.DimensionStyles(1) ' getting the Style object of the CenterMarks collection object Set objCMStyle = objCenterMarks.Style ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objCenterMarks = Nothing Set objCMStyle = Nothing End Sub