| Solid Edge FrameworkSupport Type Library : ChamferGeometry2d Object |
GetConnectedObjects | Returns both objects connected to the referenced fillet or chamfer. |
ModifyByPointAndAngle | Modifies the Chamfer object by specifying a point through which it should pass and its angle relative to the first object to which it connects. |
ModifyBySetBacks | Modifies the Chamfer object by changing its setbacks relative to the two connected objects. |
Angle | Sets and returns the angular rotation of the referenced object. |
SetBackA | Sets and returns the offset from the end of the first object to which the referenced chamfer connects. |
SetBackB | Sets and returns the offset from the end of the second object to which the referenced chamfer connects. |