Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objCircs As SolidEdgeFrameworkSupport.Circles2d
    Dim objCirc1 As SolidEdgeFrameworkSupport.Circle2d
    Dim x As Double, y As Double, z As Double
    Dim cKPType As KeyPointType
    Dim cHndType As HandleType
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create a Circles collection object
    Set objCircs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)).Circles2d
    ' Create a Circle object
    Set objCirc1 = objCircs.AddByCenterRadius(x:=0, y:=0, Radius:=0.01)
    ' Reset the KeyPoint of the circle
    Call objCirc1.SetKeyPoint(Index:=0, x:=0.05, y:=0.05, z:=0)
    ' Get a KeyPoint of the Circle
    Call objCirc1.GetKeyPoint(Index:=0, x:=x, y:=y, z:=z, KeyPointType:= _
                              cKPType, HandleType:=cHndType)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objCircs = Nothing
    Set objCirc1 = Nothing
End Sub