Solid Edge FrameworkSupport Type Library
CircularPattern2d Object Members
Overview 
Public Methods
Public Method GetGeometryReturns the geometry for the referenced pattern object.
Public Properties
Public Property AngularSpacingSets and returns the angular spacing between pattern occurrences.
Public Property ApplicationReturns the active application object.
Public Property CountReturns the number of objects in the referenced collection.
Public Property GeometryTypeReturns the type of the geometry for the referenced CircularPattern2d object.
Public Property LayerSets and returns the named layer on which the referenced object resides.
Public Property OffsetTypeSets and returns the offset type for the referenced pattern object.
Public Property ParentReturns the parent object for the referenced object.
Public Property ReferenceOccurrenceSets and returns the pattern occurrence that serves as the reference occurrence.
Public Property SuppressedSpecifies whether or not the referenced pattern object is suppressed.
Public Property TypeSpecifies the type of the object being referenced.
See Also

CircularPattern2d Object

Send comments on this topic.