Solid Edge FrameworkSupport Type Library
SetEndPoint Method
Specifies the coordinates of the end point.
Specifies the coordinates of the end point.
Specifies the coordinates of the end point.
Description
Syntax
Visual Basic
Public Sub SetEndPoint( _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal z As Double _
) 
Parameters
x
Specifies the coordinates of the end point.
y
Specifies the coordinates of the end point.
z
Specifies the coordinates of the end point.
See Also

Connector Object  | Connector Members  | Solid Edge V18 - What's New

Send comments on this topic.