Solid Edge FrameworkSupport Type Library
AddCornerAnnotation Method
Description
Creates a CornerAnnotation. For creating PMI CornerAnnotation a plane must be set (XY plane is the default). The collection object from which it is derived (sheet/profile2d/PMI) dictate the creation of CornerAnnotation.
Syntax
Visual Basic
Public Function AddCornerAnnotation( _
   ByVal AnnotInitData As AnnotInitData _
) As CornerAnnotation
Parameters
AnnotInitData
See Also

CornerAnnotations Collection  | CornerAnnotations Members  | Solid Edge ST5 - What's New

Send comments on this topic.