Solid Edge FrameworkSupport Type Library
BreakLineDistance Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
CornerAnnotation Object
: BreakLineDistance Property
Description
Sets and returns the length along the x axis that the break line traverses.
Property type
Read-write property
Syntax
Visual Basic
Public Property BreakLineDistance As Double
Remarks
This property is only enabled if the BreakLine property is True.
See Also
CornerAnnotation Object
|
CornerAnnotation Members
Send comments
on this topic.