Solid Edge FrameworkSupport Type Library
AddDatumFrame Method
Description
Creates a DatumFrame. For creating PMI DatumFrames a plane must be set (XY plane is the default). The collection object from which it is derived (sheet/profile2d/PMI) dictate the creation of DatumFrame.
Syntax
Visual Basic
Public Function AddDatumFrame( _
   ByVal AnnotInitData As AnnotInitData _
) As DatumFrame
Parameters
AnnotInitData
See Also

DatumFrames Collection  | DatumFrames Members  | Solid Edge ST5 - What's New

Send comments on this topic.