Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatums As SolidEdgeFrameworkSupport.DatumFrames
    Dim objDtmFrm1 As SolidEdgeFrameworkSupport.DatumFrame
    Dim objDtmFrm2 As SolidEdgeFrameworkSupport.DatumFrame
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Create a DatumFrames collection object
    Set objDatums = objSheet.DatumFrames
    ' Add a DatumFrame object
    Set objDtmFrm1 = objDatums.Add(x1:=0.1, y1:=0.1, z1:=0)
    ' Assign the Text to the DatumFrame
    objDtmFrm1.Datum = "Test"
    ' Assign the DatumFrame object created to another object
    Set objDtmFrm2 = objDatums.Item(Index:=1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatums = Nothing
    Set objDtmFrm1 = Nothing
    Set objDtmFrm2 = Nothing
End Sub