Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objDatums As SolidEdgeFrameworkSupport.DatumFrames
Dim objDtmFrm As SolidEdgeFrameworkSupport.DatumFrame
Dim objLine As SolidEdgeFrameworkSupport.Line2d
Dim dblBreakLineDist As Double
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Get the Active Sheet object
Set objSheet = objDoc.ActiveSheet
' Create a Line object
Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.2, y2:=0.1)
' Create a DatumFrames collection object
Set objDatums = objSheet.DatumFrames
' Add a DatumFrame object
Set objDtmFrm = objDatums.AddByTerminator(TerminatorObject:=objLine, _
x1:=0.15, y1:=0.1, z1:=0, keyPoint1:=False)
objDtmFrm.Datum = "Test"
' Add Vertex to the object
Call objDtmFrm.AddVertex(x:=0.3, y:=0.2, z:=0)
Call objDtmFrm.AddVertex(x:=0.4, y:=0.1, z:=0)
' Set the BreakLine property to true
objDtmFrm.BreakLine = True
' Get the initial BreakLine Distance
dblBreakLineDist = objDtmFrm.BreakLineDistance
' Assign a new Distance value
objDtmFrm.BreakLineDistance = 0.02
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objDatums = Nothing
Set objDtmFrm = Nothing
Set objLine = Nothing
End Sub