| Solid Edge FrameworkSupport Type Library > DatumFrame Object : Style Property | 
| Visual Basic | 
|---|
| Public Property Style As DimStyle | 
Private Sub Form_Load() Dim objApp As SolidEdgeFrameWork.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objDatums As SolidEdgeFrameworkSupport.DatumFrames Dim objDtmFrm As SolidEdgeFrameworkSupport.DatumFrame Dim objANSIDimStyle As SolidEdgeFrameworkSupport.DimensionStyle Dim objDimStyles As SolidEdgeFrameworkSupport.DimensionStyles Dim objDtmFrmStyle As SolidEdgeFrameworkSupport.DimStyle Dim strDimStyleName As String, strParentName As String ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If 'Get the Active Sheet object Set objSheet = objDoc.ActiveSheet ' Create a DatumFrames collection object Set objDatums = objSheet.DatumFrames 'Get the DimensionsStyles collection object Set objDimStyles = objDoc.DimensionStyles strDimStyleName = "ANSIDimStyle" strParentName = "ANSI" 'Create a DimStyle with ANSI as parent style Set objANSIDimStyle = objDimStyles.Add(Name:=strDimStyleName, Parent:=strParentName) ' Assign a Style property to the DatumFrames objDatums.Style = objANSIDimStyle ' Add a DatumFrame object Set objDtmFrm = objDatums.Add(x1:=0.1, y1:=0.1, z1:=0) ' Assign the Text to the DatumFrame objDtmFrm.Datum = "Test" ' Get the Style property of the DatumFrame object Set objDtmFrmStyle = objDtmFrm.Style ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objDatums = Nothing Set objDtmFrm = Nothing Set objANSIDimStyle = Nothing Set objDimStyles = Nothing Set objDtmFrmStyle = Nothing End Sub