Solid Edge FrameworkSupport Type Library
AddDatumPoint Method
Description
Creates a DatumPoint. For creating PMI DatumPoints a plane must be set (XY plane is the default). The collection object from which it is derived (sheet/profile2d/PMI) dictate the creation of DatumPoint.
Syntax
Visual Basic
Public Function AddDatumPoint( _
   ByVal AnnotInitData As AnnotInitData _
) As DatumPoint
Parameters
AnnotInitData
See Also

DatumPoints Collection  | DatumPoints Members  | Solid Edge ST5 - What's New

Send comments on this topic.