Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
    Dim objdatumpoint1 As SolidEdgeFrameworkSupport.DatumPoint
    Dim objdatumpoint2 As SolidEdgeFrameworkSupport.DatumPoint
    Dim lngZorder1 As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create a collection of datumpoints
    Set objDatumPoints = objSheet.DatumPoints
    'add a datumpoint to collection
    Set objdatumpoint1 = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    'add one more datumpoint to collection
    Set objdatumpoint2 = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    'get zorder
    lngZorder1 = objdatumpoint1.ZOrder
    'Bringforward datumpoint1
    Call objdatumpoint1.BringForward
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumPoints = Nothing
    Set objdatumpoint1 = Nothing
    Set objdatumpoint2 = Nothing
End Sub