Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As solidedgedraft.DraftDocument
    Dim objSheet As solidedgedraft.Sheet
    Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
    Dim objdatumPoint As SolidEdgeFrameworkSupport.DatumPoint
    Dim objCircle As SolidEdgeFrameworkSupport.Circle2d
    Dim objCenterObj As SolidEdgeFrameworkSupport.Circle2d
    Dim dblX As Double, dblY As Double, dblZ As Double
    Dim bKeyPoint As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create a collection of datumpoint.
    Set objDatumPoints = objSheet.DatumPoints
    'draw a circle
    Set objCircle = objSheet.Circles2d.AddByCenterRadius(x:=0.2, _
                                                         y:=0.2, Radius:=0.05)
    'add a datumpoint to collection
    Set objdatumPoint = objDatumPoints.AddByElement(terminatorobject:= _
                                                    objCircle, x1:=0.2, y1:=0.2, z1:=0, keypoint1:=True)
    'call getelement
    Call objdatumPoint.GetElement(CenterObj:=objCenterObj, x:=dblX, _
                                  y:=dblY, z:=dblZ, Keypoint:=bKeyPoint)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumPoints = Nothing
    Set objdatumPoint = Nothing
    Set objCircle = Nothing
    Set objCenterObj = Nothing
End Sub