Solid Edge FrameworkSupport Type Library
Index Property
Description
Returns the numeric index for the active object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Index As Long
Remarks
This index is the sequence that the object holds in its collection object (as held by the parent).
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
    Dim objDatumPoint As SolidEdgeFrameworkSupport.DatumPoint
    Dim lngIndex As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create datumpoints collection
    Set objDatumPoints = objSheet.DatumPoints
    'add a datumpoint to collection
    Set objDatumPoint = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    'get index
    lngIndex = objDatumPoint.Index
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumPoints = Nothing
    Set objDatumPoint = Nothing
End Sub
See Also

DatumPoint Object  | DatumPoint Members

Send comments on this topic.