Solid Edge FrameworkSupport Type Library
SendBackward Method
Description
Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Syntax
Visual Basic
Public Sub SendBackward() 
Remarks
This command is useful when objects are hiding other objects that have a lower priority display but when you do not want to send the object all the way to the back of the priority list.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
    Dim objDatumPoint1 As SolidEdgeFrameworkSupport.DatumPoint
    Dim objDatumPoint2 As SolidEdgeFrameworkSupport.DatumPoint
    Dim lngZorder As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create a datumpoints' collection.
    Set objDatumPoints = objSheet.DatumPoints
    'add 2 datumpoints to collection
    Set objDatumPoint1 = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    Set objDatumPoint2 = objDatumPoints.Add(x1:=0.2, y1:=0.21, z1:=0)
    'get zorder
    lngZorder = objDatumPoint2.ZOrder
    'send backward
    Call objDatumPoint2.SendBackward
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumPoints = Nothing
    Set objDatumPoint1 = Nothing
    Set objDatumPoint2 = Nothing
End Sub
See Also

DatumPoint Object  | DatumPoint Members

Send comments on this topic.