Solid Edge FrameworkSupport Type Library
SetElement Method
Specifies the nonlinear object to which the datum point is associated.
Specifies the coordinates of the center point of the referenced object.
Specifies the coordinates of the center point of the referenced object.
Specifies the coordinates of the center point of the referenced object.
Specifies whether the DatumPoint was placed with respect to the object (True) or with respect to a key point of the object (False).
Description
Sets the element for the referenced DatumPoint object.
Syntax
Visual Basic
Public Sub SetElement( _
   ByVal CenterObj As Object, _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal z As Double, _
   ByVal keyPoint As Boolean _
) 
Parameters
CenterObj
Specifies the nonlinear object to which the datum point is associated.
x
Specifies the coordinates of the center point of the referenced object.
y
Specifies the coordinates of the center point of the referenced object.
z
Specifies the coordinates of the center point of the referenced object.
keyPoint
Specifies whether the DatumPoint was placed with respect to the object (True) or with respect to a key point of the object (False).
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
    Dim objdatumPoint As SolidEdgeFrameworkSupport.DatumPoint
    Dim objCircle1 As SolidEdgeFrameworkSupport.Circle2d
    Dim objCircle2 As SolidEdgeFrameworkSupport.Circle2d
    Dim objCenterObj As SolidEdgeFrameworkSupport.Circle2d
    Dim dblX As Double, dblY As Double, dblZ As Double
    Dim bKeyPoint As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create a collection of datumpoint.
    Set objDatumPoints = objSheet.DatumPoints
    'draw circles
    Set objCircle1 = objSheet.Circles2d.AddByCenterRadius(x:=0.2, _
                                                          y:=0.2, Radius:=0.05)
    'add a datumpoint to collection
    Set objdatumPoint = objDatumPoints.AddByElement(terminatorobject:= _
                                                    objCircle1, x1:=0.2, y1:=0.2, z1:=0, keypoint1:=True)
    'Draw another cirlce to be set as element for the DatumPoint
    Set objCircle2 = objSheet.Circles2d.AddByCenterRadius(x:=0.3, _
                                                          y:=0.3, Radius:=0.05)
    'setelement
    Call objdatumPoint.SetElement(CenterObj:=objCircle2, x:=0.3, _
                                  y:=0.3, z:=0, Keypoint:=True)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumPoints = Nothing
    Set objdatumPoint = Nothing
    Set objCircle1 = Nothing
    Set objCircle2 = Nothing
    Set objCenterObj = Nothing
End Sub
See Also

DatumPoint Object  | DatumPoint Members

Send comments on this topic.