Solid Edge FrameworkSupport Type Library
SetKeyPoint Method
Specifies the index of the key point/handle.
Specifies the x coordinate of the specified key point.
Specifies the y coordinate of the specified key point.
Specifies the z coordinate of the specified key point.
Description
Sets the position for a specified key point.
Syntax
Visual Basic
Public Sub SetKeyPoint( _
   ByVal Index As Long, _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal z As Double _
) 
Parameters
Index
Specifies the index of the key point/handle.
x
Specifies the x coordinate of the specified key point.
y
Specifies the y coordinate of the specified key point.
z
Specifies the z coordinate of the specified key point.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
    Dim objDatumPoint As SolidEdgeFrameworkSupport.DatumPoint
    Dim dblX As Double, dblY As Double, dblZ As Double
    Dim cKeyPtType As SolidEdgeConstants.KeyPointType
    Dim cHandleType As SolidEdgeConstants.HandleType
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create datumpoints collection
    Set objDatumPoints = objSheet.DatumPoints
    'add a datumpoint to collection
    Set objDatumPoint = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    'setkeypoint
    Call objDatumPoint.SetKeyPoint(Index:=0, x:=0.23, y:=0.23, z:=0)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumPoints = Nothing
    Set objDatumPoint = Nothing
End Sub
See Also

DatumPoint Object  | DatumPoint Members

Send comments on this topic.