Solid Edge FrameworkSupport Type Library
AddDatumTarget Method
Description
Creates a DatumTarget. For creating PMI DatumTarget a plane must be set (XY plane is the default). The collection object from which it is derived (sheet/profile2d/PMI) dictate the creation of DatumTarget.
Syntax
Visual Basic
Public Function AddDatumTarget( _
   ByVal AnnotInitData As AnnotInitData _
) As DatumTarget
Parameters
AnnotInitData
See Also

DatumTargets Collection  | DatumTargets Members  | Solid Edge ST5 - What's New

Send comments on this topic.