| Solid Edge FrameworkSupport Type Library > DatumTargets Collection : Style Property |
| Visual Basic |
|---|
Public Property Style As DimensionStyle |
Private Sub Form_Load() Dim objApp As SolidEdgeFrameWork.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets Dim objANSIStyle As SolidEdgeFrameworkSupport.DimensionStyle Dim objStyle As SolidEdgeFrameworkSupport.DimensionStyle ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If 'getting the Active Sheet object Set objSheet = objDoc.ActiveSheet 'Getting the DatumTargets object Set objDatumTargets = objSheet.DatumTargets 'Create a dimension style Set objANSIStyle = objDoc.DimensionStyles.Add(Name:="MyDimStyle", Parent:="ANSI") 'Set the DatumTargets Style to ANSI objDatumTargets.Style = objANSIStyle 'Get the Style associated with the DatumTargets Set objStyle = objDatumTargets.Style ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objDatumTargets = Nothing Set objANSIStyle = Nothing Set objStyle = Nothing End Sub