Solid Edge FrameworkSupport Type Library
AngularDMSRoundOff Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimStyle Object
: AngularDMSRoundOff Property
Description
Sets and return the angular round off when angular units is set to Deg-Min-Sec.
Property type
Read-write property
Syntax
Visual Basic
Public Property AngularDMSRoundOff As
DimDMSRoundOffTypeConstants
Remarks
Valid values are members of the DimDMSRoundOffTypeConstants constant set.
See Also
DimStyle Object
|
DimStyle Members
Send comments
on this topic.