Solid Edge FrameworkSupport Type Library
AngularUnits Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimStyle Object
: AngularUnits Property
Description
Sets and returns the angular dimensioning unit separate from the working units of the file.
Property type
Read-write property
Syntax
Visual Basic
Public Property AngularUnits As
DimAngularUnitConstants
Remarks
Valid values are members of the DimAngularUnitConstants constant set.
See Also
DimStyle Object
|
DimStyle Members
Send comments
on this topic.