Solid Edge FrameworkSupport Type Library
CoordinateAutoJog Property
Description
Determines if the referenced coordinate dimension is jogged automatically when the dimension value is less than the coordinate stack pitch.
Property type
Read-write property
Syntax
Visual Basic
Public Property CoordinateAutoJog As Boolean
See Also

DimStyle Object  | DimStyle Members

Send comments on this topic.