Solid Edge FrameworkSupport Type Library
CoordinateStackPitch Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimStyle Object
: CoordinateStackPitch Property
Description
Sets and returns the minimum coordinate dimension value after which the coordinate dimension will be jogged when the CoordAutoJog property is set to True.
Property type
Read-write property
Syntax
Visual Basic
Public Property CoordinateStackPitch As Double
See Also
DimStyle Object
|
DimStyle Members
Send comments
on this topic.