Solid Edge FrameworkSupport Type Library
HorizontalToleranceGap Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimStyle Object
: HorizontalToleranceGap Property
Description
Sets and returns the horizontal tolerance gap between the dimension value and tolerance text.
Property type
Read-write property
Syntax
Visual Basic
Public Property HorizontalToleranceGap As Double
Remarks
The value is ratio to text.
See Also
DimStyle Object
|
DimStyle Members
Send comments
on this topic.