Solid Edge FrameworkSupport Type Library
MaximumSubunits Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimStyle Object
: MaximumSubunits Property
Description
Sets and returns the maximum number of subunits displayed by the associated dimension before truncating and adding to the unit.
Property type
Read-write property
Syntax
Visual Basic
Public Property MaximumSubunits As Integer
See Also
DimStyle Object
|
DimStyle Members
Send comments
on this topic.