Solid Edge FrameworkSupport Type Library
MaximumViewAngle Property
Description
Sets and returns the maximum view angle after which the associated dimension will not be displayed in a 3-D environment.
Property type
Read-write property
Syntax
Visual Basic
Public Property MaximumViewAngle As Double
See Also

DimStyle Object  | DimStyle Members

Send comments on this topic.