Solid Edge FrameworkSupport Type Library
TerminatorDisplay Property
Description
Gets/Sets the Terminator Display.
Property type
Read-write property
Syntax
Visual Basic
Public Property TerminatorDisplay As DimTermDisplayTypeConstants
Remarks
This property can be set to display the origin, measurement, none, or both terminators in a dimension. Valid values are members of the DimTermDisplayTypeConstants constant set.
See Also

DimStyle Object  | DimStyle Members

Send comments on this topic.