Toggles the associated dimension to the outside of the projection when the dimension value is less than the terminator inside limit.
Property type
Read-write property
Syntax
Visual Basic
Public Property TerminatorInsideLimit As Double
Remarks
When the dimension value is less than the value of the TerminatorInsideLimit property (specified as a ratio of text height), the associated dimension is automatically positioned outside of the projection.