Solid Edge FrameworkSupport Type Library
VerticalToleranceGap Property
Description
Sets and returns the vertical tolerance gap between the dimension value and the tolerance text.
Property type
Read-write property
Syntax
Visual Basic
Public Property VerticalToleranceGap As Double
Remarks
The value is ratio to text.
See Also

DimStyle Object  | DimStyle Members

Send comments on this topic.