Solid Edge FrameworkSupport Type Library
Dimension Object
Members
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
: Dimension Object
Description
Stores characteristics such as size, distance, and angle.
Object Model
Remarks
The dimensioning objects are associative to the geometry they are measuring. The Dimension object is created only through the Dimensions collection object.
See Also
Dimension Members
Send comments
on this topic.