Solid Edge FrameworkSupport Type Library
Parent Property
Description
Returns the parent object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Parent As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objDimStyles As SolidEdgeFrameworkSupport.DimensionStyles
    Dim objDimStylesParent As SolidEdgeDraft.DraftDocument
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the DimensionsStyles collection object
    Set objDimStyles = objDoc.DimensionStyles
    'Get the Application object from DimStyles collection object
    Set objDimStylesParent = objDimStyles.Parent
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objDimStyles = Nothing
    Set objDimStylesParent = Nothing
End Sub
See Also

DimensionStyles Collection  | DimensionStyles Members

Send comments on this topic.