Solid Edge FrameworkSupport Type Library
Remove Method
Specifies the name of the item to be removed.
Description
Removes a specified object from the referenced collection.
Syntax
Visual Basic
Public Sub Remove( _
   ByVal Name As String _
) 
Parameters
Name
Specifies the name of the item to be removed.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objDimStyles As SolidEdgeFrameworkSupport.DimensionStyles
    Dim objANSImmDimStyle As SolidEdgeFrameworkSupport.DimensionStyle
    Dim lngCount As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the DimensionsStyles collection object
    Set objDimStyles = objDoc.DimensionStyles
    'Get the Count of DimStyles
    lngCount = objDimStyles.Count
    'Add a New DimStyle
    Set objANSImmDimStyle = objDimStyles.Add(Name:="DimStyle1", Parent:="ANSImm")
    'Remove the newly created DimStyle
    objDimStyles.Remove Name:="DimStyle1"
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objDimStyles = Nothing
    Set objANSImmDimStyle = Nothing
End Sub
See Also

DimensionStyles Collection  | DimensionStyles Members

Send comments on this topic.