Solid Edge FrameworkSupport Type Library
AboveGap Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimensionStyle Object
: AboveGap Property
Description
Sets and returns the gap between the dimension text and the dimension line when the text position is set to above.
Property type
Read-write property
Syntax
Visual Basic
Public Property AboveGap As Double
Remarks
The value is ratio to text.
See Also
DimensionStyle Object
|
DimensionStyle Members
Send comments
on this topic.