Solid Edge FrameworkSupport Type Library
AngularDMSRoundOff Property
Description
Sets and return the angular round off when angular units is set to Deg-Min-Sec.
Property type
Read-write property
Syntax
Visual Basic
Public Property AngularDMSRoundOff As DimDMSRoundOffTypeConstants
Remarks
Valid values are members of the DimDMSRoundOffTypeConstants constant set.
See Also

DimensionStyle Object  | DimensionStyle Members

Send comments on this topic.