Solid Edge FrameworkSupport Type Library
AngularDecimalRoundOff Property
Description
Sets and returns the angular round-off when angular units is set to degrees or radians and round off type is set to decimal.
Property type
Read-write property
Syntax
Visual Basic
Public Property AngularDecimalRoundOff As DimDecimalRoundOffTypeConstants
Remarks
Valid values are members of the DimDecimalRoundOffTypeConstants constant set.
See Also

DimensionStyle Object  | DimensionStyle Members

Send comments on this topic.