Solid Edge FrameworkSupport Type Library
AngularFractionRoundOff Property
Description
Sets and returns the angular round off when angular units is set to degrees or radians and round off type is set to fraction.
Property type
Read-write property
Syntax
Visual Basic
Public Property AngularFractionRoundOff As DimFractionRoundOffTypeConstants
Remarks
Valid values are members of the DimFractionRoundOffTypeConstants constant set.
See Also

DimensionStyle Object  | DimensionStyle Members

Send comments on this topic.