Solid Edge FrameworkSupport Type Library
AutoSuppressDiameter Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimensionStyle Object
: AutoSuppressDiameter Property
Description
Specifies whether or not to automatically suppress the diameter symbol when a circle is measured by a radial or circular diameter dimension.
Property type
Read-write property
Syntax
Visual Basic
Public Property AutoSuppressDiameter As Boolean
See Also
DimensionStyle Object
|
DimensionStyle Members
Send comments
on this topic.