Solid Edge FrameworkSupport Type Library
DatumFrameDashes Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimensionStyle Object
: DatumFrameDashes Property
Description
Sets and returns the datum frame dashes for the referenced DatumFrame object.
Property type
Read-write property
Syntax
Visual Basic
Public Property DatumFrameDashes As Boolean
Remarks
When this property is True, dashes are automatically drawn before and after the datum text.
See Also
DimensionStyle Object
|
DimensionStyle Members
Send comments
on this topic.