Solid Edge FrameworkSupport Type Library
DrivingColor Property
Description
Sets and returns the color in which driving dimensions are displayed.
Property type
Read-write property
Syntax
Visual Basic
Public Property DrivingColor As Long
Remarks
When an equation constraint is assigned to make a driving dimension a function of another dimension, a variable, or an equation, the color of the text of the driving dimension will assume the driven dimension color. If the relationship is removed, the text again assumes the driving dimension color.
See Also

DimensionStyle Object  | DimensionStyle Members

Send comments on this topic.