Solid Edge FrameworkSupport Type Library
MaximumViewAngle Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimensionStyle Object
: MaximumViewAngle Property
Description
Sets and returns the maximum view angle after which the associated dimension will not be displayed in a 3-D environment.
Property type
Read-write property
Syntax
Visual Basic
Public Property MaximumViewAngle As Double
See Also
DimensionStyle Object
|
DimensionStyle Members
Send comments
on this topic.