Solid Edge FrameworkSupport Type Library
ProjectionOffsetGap Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimensionStyle Object
: ProjectionOffsetGap Property
Description
Sets and returns the gap between the object being measured and the projection line.
Property type
Read-write property
Syntax
Visual Basic
Public Property ProjectionOffsetGap As Double
Remarks
he projection offset gap value is a ratio of dimension text height.
See Also
DimensionStyle Object
|
DimensionStyle Members
Send comments
on this topic.