Solid Edge FrameworkSupport Type Library
SecondaryToleranceEquivalent Property
Description
Specifies whether or not the secondary tolerance is equivalent.
Property type
Read-write property
Syntax
Visual Basic
Public Property SecondaryToleranceEquivalent As Boolean
Remarks
If SecondaryToleranceEquivalent is True (the default), then secondary tolerances are computed from the primary tolerances.
See Also

DimensionStyle Object  | DimensionStyle Members

Send comments on this topic.