Imports System.Runtime.InteropServices
Public Class SmartDepthSlotFinite
    Private Sub btnSmartDepthSlotFinite_Click(sender As System.Object, e As System.EventArgs) Handles btnSmartDepthSlotFinite.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
        Dim objDimStyles As SolidEdgeFrameworkSupport.DimensionStyles = Nothing
        Dim objTempStyle As SolidEdgeFrameworkSupport.DimensionStyle = Nothing
        Dim objType As Type = Nothing
        Dim strFiniteSlot As String
        Try
            ' Create/get the application with specific settings
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            If objApplication Is Nothing Then
                ' Get the type from the Solid Edge ProgID
                objType = Type.GetTypeFromProgID("SolidEdge.Application")
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(objType)
                ' Make Solid Edge visible
                objApplication.Visible = True
            End If
            objDraftDoc = objApplication.ActiveDocument
            'Get the DimensionsStyles collection object
            objDimStyles = objDraftDoc.DimensionStyles
            'Get reference to first DimStyle.
            objTempStyle = objDimStyles(0)
            'Set the smart depth for Finite slot
            objTempStyle.SmartDepthSlotFinite = "%HD - DEEP"
            'Get the smart depth for Finite slot
            strFiniteSlot = objTempStyle.SmartDepthSlotFinite
            If strFiniteSlot <> "%HD - DEEP" Then
                MsgBox("Error in SmartDepthSlotFinite property for dimension style.")
            End If
        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub
End Class